Trane Worldwide Sites
Trane specializes in the intangible, invisible factor that is critical to the mission of higher education: indoor air quality (IAQ). Trane solutions enable you to properly (and precisely) manage air cleaning, air conditioning and heating, and humidity levels to suit specific applications throughout your campus—in new and old buildings.
Trane can help deliver an exceptional educational value by maximizing operational cost reduction through improved energy efficiency while providing the ultimate learning environment.
Effective classrooms
Numerous studies, including those
conducted by the IAQ Scientific Findings Resource Bank (SFRB), a
cooperative venture between EPA and the Lawrence Berkeley National
Laboratory, have shown that ideal IAQ improves the performance of
mental tasks, including concentration and recall. Trane technologies
establish and maintain proper IAQ.
Lab safety and productivity
Research labs are vital to
your reputation and revenue stream, but they have the potential to
produce air quality hazards, and they may fall under the jurisdiction
of health regulations. Meanwhile, sensitive instruments and
experiments may require precisely controlled temperature and humidity
levels. Further complicating the matter: laboratories must be revised
every few years as current projects end and new researchers take over
the space.
Trane provides solutions to ensure that IAQ levels support lab
safety and research success. Our flexible applications can
accommodate changing project requirements with a few quick and easy modifications.
Archive preservation
Colleges and universities are the
keepers of history and legacy. Trane can control precise humidity and
temperature conditions for optimum document preservation and the
safekeeping of priceless artwork and historical artifacts. CDQ™
dessicant dehumidification from Trane keeps buildings cool, dry
and quite while incurring less energy cost. This is an ideal
technology to implement in areas where humidity control is critical,
including libraries, museums and galleries.
Building new or renovating existing residence halls and athletic facilities is one of the best ways to attract students to your school, and to keep more students living on campus. These campus facilities can also promote student health and wellness. However, you need to take more than aesthetics into consideration. The most important upgrades are not always visible.
Trane offers innovative and energy-efficient solutions for improving IAQ in residence halls, athletic facilities and student union buildings—wherever students gather in large numbers or close quarters. For example, equipping air handlers with a Trane Catalytic Air Cleaning System (TCACS) effectively reduces biological organisms such as spores, bacteria and even the tiniest viruses.